This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4403EVM: EVM sensor provide and GUI question

Part Number: AFE4403EVM

Dear all,

1. May I ask if there are other sensor board versions available for evaluation, such as OSRAM 7060 or OSRAM 7072?

2. Regarding continuous measurement data logging: based on the file content, it seems the system stores data from the beginning to the end of the full measurement duration. Is it possible to only store the data within the displayed window range instead of the entire measurement period?

  • Hello Frank,

    1) The AFE4403EVM is only designed to interface with the OSRAM SFH7050 sensor. There are no other versions of the EVM available to evaluate with other sensor boards.

    2) In order to capture only the data that is included in the GUI's plot, you have to be in the "Finite" data capture mode. In "Continuous" capture mode, you will need to manually trim the data after export to isolate only the data shown in the GUI's plot.

    The menu in the "ADC Capture and Analysis" window of the AFE4403EVM GUI. The "Capture Mode" dropdown is set to "Finite," which is emphasized with a bold red box surrounding it.

    Regards,

    Payton