Part Number: DAC80501
Dear Sir or Madam,
We are using your DAC80501 with an external reference of 4.096 V. Please find the schematic attached.
As you can see from the attached waveform plots, there appears to be a linearity issue in the range between 0.0 V and 0.02 V. As a simple example, we programmed a triangular waveform oscillating between 0 V and 62 mV. Below 10 mV, the waveform is clearly non-linear. This behavior does not occur at the upper transition point.
When we apply an offset of approximately 20 mV to the entire signal, these non-linearities disappear entirely. This confirms that the issue is strictly limited to the very bottom of the output range.
Based on the datasheet, we would expect significantly better linearity performance. This was also one of the main reasons we chose this device.
Question 1: Is there anything we may have overlooked in the datasheet, and is this behavior expected from the DAC?
Question 2: What can we do to improve the linearity in this low-voltage range?
Thank you very much and kind regards, Dan
Attachments:
-
Schematic
-
Distorted triangle waveform
-
Correct triangle waveform with offset
-
Distorted sine waveform
-
Correct sine waveform with offset