I don't understand the "Modulator Noise Spectrum" figure in the ADS1298 datasheet (Fig 29).
It says it's showing Normalized Frequency, but what was the frequency normalized by?
Usually "normalized" frequencies are unitless, but it says the units are Hz and the x-axis shows data up to 700Hz.
The figure title says "Modulator Noise Spectrum Up To 0.5 × fMOD," but fMOD is either 256kHz or 512kHz depending on the operating mode (Low Power/High Resolution).
Can someone make sense of this?
Thanks!