Part Number: ADC3644EVM
Other Parts Discussed in Thread: TSWDC155EVM
We received both the ADC3644EMV and TSWDC155EVM. On a Windows 11 machine, installed the ADC36xxEVM GUI V1.1.1, HSDC Pro v5.31 and have Vivaldo 2022.2 installed. The USB-C ports on both EVM's, A JTAG programmer connected to J2 of the TSWDC155EVM, CLKp in at 65MHz +10dBm, DCLK 227.5MHz +10dBm, and 12V on the power connector. The HSDC Pro was opened before the ADC36xxEVM. The power and status lights did come on.
In the GUI when it is up, a sample frequency of 65MHz is entered. Calculate is pressed and it shows 227.5MHz for the DCLK frequency. After that the "Program" button is selected. And after a short time, the error message ADC36xxEVM_CMOS' object has no attribute 'tswdc155evm' comes up. It appears that the Python code running under this GUI does not have a tswdc155evm object.
What is mssing in this installation, or is there a different ADC36xxEVM GUI I need to install?