This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE782H1: HART response Data transmitted from MCU received at host are not in order.

Part Number: AFE782H1

Hi,

We have setup AFE782H1 for DAC + HART using SPI communication. The responses from the MCU are sent to HART Modem when sniffed on a serial port looks like a part of previous response is sent along with the current response data, missing few bytes. These missed bytes from current response are seen transmitted in the next data transmission.

For now I'm flusing the Transmit FIFO buffer every time before sensing the response. However, is there a way to correct this without explicitly flusing the buffer every time.

 

Regards,

Abdul