Part Number: DAC34H84
I like to check the output frequency range of DAC34H84.
I understand that it may also determined by the output stage after the DAC. Our output stage is working fine.
We are having issue to get the outputs in SYNC or aligned for the frequency below 5MHz, even from the same device.
Our sampling clock is 100MHz and signal should from 3 to 30 MHz. It's fine (in SYNC) above 5MHz (5to 30 MHz). The output A and C are used.
Was there any restriction for lower frequencies on this devce? Hope to hear from you ASAP. Thank you.