Part Number: ADS131E06
Customer has noticed what appears to be a DC offset in the FFT associated with the ADS131E06, see Fig 10 of the datasheet:
My understanding is, this figure shows an FFT of ADC output when ADC input is presented with a pure 0dBFS 60 Hz sine wave (meaning, that sine wave should have zero DC offset).
The question is: is there really a spike in the plot at 0 Hz, and if so, what's the nature of it? Is that simply a DC offset of the ADC (which is already characterized by the datasheet, but hasn't been calibrated out when making a plot), or is it some additional DC error induced by the presence of AC signal, kind of a result of nonlinear distortion of the AC signal?
If it's the latter, that means this error has to be proportional to the level of the AC signal (or a certain power thereof...). Do you have some way to quantify it? I'd like to understand the nature of it, and to factor that into our error calculations.