This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1306E05: Decoding Manchester output AMC1306E05

Part Number: AMC1306E05
Other Parts Discussed in Thread: AMC1306M05

We have AMC1306E05 connected to controller where we using sinc3 filter to decode and filter the manchester output stream of AMC1306E05. We are not seeing the promising result with the given configuration as the resutls varies graltely if we use diffrent decimation factor or the clock frequency (CLKIN for AMC1306E0). 

Since both the AMC1306E05 and the controller’s filtering (decoding and Sinc3 filter) are treated as black boxes in our setup, we want to validate the behavior of the AMC1306E05 independently.

The AMC1306E05 datasheet does not provide detailed information about the bitstream output for different input voltages. Section 8.3.4 mentions the expected stream of zeros and ones for 0 V, +250 mV, and –250 mV, but we need to validate that the actual bitstream matches the applied voltage. What would the exact bitstream look like for these voltages, and if we want to check manually, what window size should we use to calculate the percentage of zeros and ones as indicated in the datasheet?


 image.png


  • Hi Barish,

    Welcome to our e2e forum!  The 'ones density' would not change between Manchester vs. the traditional coding output.  You need to review Figure 52 to compare the uncoded versus Manchester coded bitstream.  What controller are you using to reconstruct the Manchester coded output?  

  • Hello Tom, 
    Thank you for the response. 

    We are using STM32U5XX and using the MDF (multifunction digital filter) peripheral/module of controller.
    We also have results for different differential input voltage applied to AMC1306E05 with different filters, decimation factor and the clock as follows:

    1) Filter = Fastsin, Decimation = 512, clock = 7.9Mhz
    12mV	      51915264
    56.7 mV	    62193561
    101.9 mV	  70359859
    147.1 mV	  58060902
    192.2 mV	  37196953
    237.4 mV	  19629875
    
    
    2) Filter = Sin3, Decimation = 16, clock = 18.1 Mhz
    12mV	     38963 
    56.7 mV	   187852 
    101.9 mV   333824 
    147.1 mV   484147 
    192.2 mV   629862 
    237.4 mV   778547 
    
    
    3) Filter = Sin3, Decimation = 32, clock = 18.1 Mhz
    12mV	     312832 
    56.7 mV	   1496012 
    101.9 mV   2681036 
    147.1 mV   3864064 
    192.2 mV   5048832 
    237.4 mV   6229555 
    
    
    4) Filter = Sin3, Decimation = 64, clock = 18.1 Mhz
    
    12mV	      2515865 
    56.7 mV	   11981721 
    101.9 mV   21450188 
    147.1 mV   30917580 
    192.2 mV   40390092 
    237.4 mV   49858201 
    
    5) Filter = Sin3, Decimation = 128, clock = 9.7 Mhz
    12mV	     208135475 
    56.7 mV	   271983667 
    101.9 mV   279499673 
    147.1 mV   186647756 
    192.2 mV   106407833 
    237.4 mV    50848153  
    
    
    6) Filter = Sin3, Decimation = 128, clock = 12.7 Mhz
    12mV	     209969305 
    56.7 mV	   267022694 
    101.9 mV   278268057 
    147.1 mV   192710246 
    192.2 mV   106398361 
    237.4 mV    50849433 
    
    7) Filter = Sin3, Decimation = 128, clock = 18.1 Mhz
    12mV	      20118732 
    56.7 mV	    95853465 
    101.9 mV   171593420 
    147.1 mV   247348224 
    192.2 mV   323098368 
    237.4 mV   398857113 
    
    
    8) Filter = Sin3, Decimation = 128, clock = 25.4 Mhz
    12mV	      20159897 
    56.7 mV	    95788185 
    101.9 mV    171539353 
    147.1 mV    247321651 
    192.2 mV    322997350 
    237.4 mV    398782668
    
    
    9) Filter = Sin3, Decimation = 256, clock = 18.1 Mhz
    
    12mV	      160983091
    56.7 mV	    463869747
    101.9 mV	  1069925632
    147.1 mV	  1675955251
    192.2 mV	  2063188403 WARNING: Filter5 SATF=1 (saturation/error detected)
    237.4 mV		2147483392 (WARNING: Filter5 SATF=1 (saturation/error detected))
    
    
    10) Filter = Sin5, Decimation = 32, clock = 7.9Mhz
    
    12mV	      2147483392 (WARNING: Filter5 SATF=1 (saturation/error detected))
    56.7 mV	    2147483392 (WARNING: Filter5 SATF=1 (saturation/error detected))
    101.9 mV	  2147483392 (WARNING: Filter5 SATF=1 (saturation/error detected))
    147.1 mV	  2132144972 (WARNING: Filter5 SATF=1 (saturation/error detected)) 
    192.2 mV	  1925125452
    237.4 mV	  1258743910
    
    
    
    11) Filter = sinc3, Decimation = 256, clock = 7.9Mhz
    12mV	      1040050892
    56.7 mV	    1919153587 (WARNING: Filter5 SATF=1 (saturation/error detected))
    101.9 mV	  2129002342 (WARNING: Filter5 SATF=1 (saturation/error detected))
    147.1 mV	  1805260697
    192.2 mV	  1200068198
    237.4 mV	  629071411
    
    
    12) Filter = sinc3, Decimation = 256, clock = 7.9Mhz
    12mV	      13024358
    56.7 mV	    12988108
    101.9 mV	  13065676
    147.1 mV	  13119232
    192.2 mV	  13061734
    237.4 mV	  13109555


    Summary of results: 

    Good: Sin3 @ 18.1 MHz (decimations 16/32/64/128), Sin3 @ 25.4 MHz (decimation 128). These climb smoothly without saturation.

    Marginal: Sin3 @ 9.7 MHz and 12.7 MHz (decimation 128) show mid-range roll-off after ~102 mV.

    Poor/saturated: Sin3 decimation 256 @ 18.1 MHz (hits SATF at high inputs), Sin5 @ 7.9 MHz (saturated almost entirely), sinc3 first set (multiple SATF), sinc3 second set (flat ~13 M across inputs), Fastsin @ 7.9 MHz (non-monotonic).

    Based on the observed results, the filter output shows inconsistencies across different decimation, filter, and clock configurations. While variations in output counts are expected, the linearity should have been maintained. We have an open query with STM to understand the root cause of this behavior.


    Our objective is to understand the expected output behavior of the AMC1306E05 for various input voltage levels


    According to Figure 52, Manchester encoding is illustrated based on the uncoded bitstream. Our question is: which bitstream (uncoded or Manchester-coded) does the AMC1306E05 output for different input voltages?
    For example, If 0 mV results in 50% ones and zeros, will the output be:
    1) A repeating pattern like (010101010101...) continuously?
    2) Blocks of 16 zeros followed by 16 ones?
    3) Larger blocks, such as 127 zeros followed by 127 ones?”

    The clarification on the bit stream will be helpful to debug the MDF implementation. 

    Thank you in advance. 

  • The AMC1306E05 uses the Manchester coded output while the M05 would use the uncoded output.  The Manchester decoding done in the CPU would need to be using a clock at least 6 times faster than the datastream.  Have you tried the AMC1306M05 as an alternate?  My understanding is that the STM32U5XX does not have a native Manchester decoder so that might be part of the issues you are having.