Part Number: ADS124S08
Other Parts Discussed in Thread: ADS1248
We configured the ADS124S08 ADC to operate in continuous conversion mode with the START pin held HIGH at all times. However, when it becomes necessary to reset the ADC during operation and a RESET command is issued, the data conversion is remains stopped even though the START pin is still HIGH.
According to the datasheet, after a reset the device enters a standby state and does not resume conversions until it detects either a rising edge on the START pin or a START command.
In this case, if the START pin is intended to remain HIGH continuously, is it correct that we should use the START command to restart data convserion?