Part Number: ADS131M06-Q1
Other Parts Discussed in Thread: ADS131M06,
Hi, im using ADS131M06,
word length set to 16bit mode
sample rate set to 32ksps, are able to do, after that im reading the data with drdy falling edge signal,
once after drdy falling edge occurs SPI transfer start , data is reading after that in the last crc frame drdy goes high, but again it is becoming low, it should become low in next sample rate only right, but before itself it is become low. what will be the reason.
please find the attached waveforms
yellow = drdy, blue = chip select , green = spi clock, in the below image we can see drdy interrupt comes every 32ksps, but in between drdy signal become high and low, i dont know why

image 2 - zoomed one

please kindly help us and suggest what to do for this issue.
regards,
srinath