This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7960: ADS7960 Schematic Review

Part Number: ADS7960

Hello,

The following is the schematic diagram of ADS7960. Could you please help me check if there are any issues? Can GPO0-3 pins float? Thanks.

image_1767877574043.jpg

  • Hello,

    The 100Ω on the SPI pins is excessive. Usually 50Ω and below is sufficient to prevent overshoot and ringing while keeping edge transitions quick.

    Unused GPIO pins can be left floating.

    The supply decoupling looks good. 

    Can you share more on what signals the analog input pins will be connected to, and do you have a schematic to share of them?

    Regards,
    Joel