Apologies for basic question, but had difficulty working through all the possibilities on the TI site
I have been wanting to build an A/D converter for electrophysiological signals (pre-amplified to arbitrarily useful voltages such as +-5V) with the following basic specs - at least 14 bit resolution, and minimum of 500k samples/second (1million preferred); minimum of 2 channels, 4 preferred, but happy to run a set of single channel chips in parallel; D/A capabilities also very useful. Power is not an issue; lowish noise is good. The ADS1248EVM-PDK looks interesting; reasonably simple software interface would be useful, perhaps to be run from Matlab, but can code in C etc. Evaluation kit much preferred.
Could I get some suggestions?
Many thanks
Chris French, University of Melbourne