Part Number: ADC3683EVM
Other Parts Discussed in Thread: ADC3683, ADC3664EVM
Dear Sir/Madam,
We are trying to establish SPI connection using the USB port on the DC134 REV E board. (which seems important because it appears there are various "ADC3683EVM" boards out there.
I've tried installing the ADC36xx-EVM-GUI version 1.2.0. when I plug in the device and then start the GUI. I get the warning:
An error occurred: 0
Traceback (most recent call last):
File "main.py", line 359, in run
KeyError: 0
In the bottom of the GUI window (that I cannot interact with) I do see "ADC35XX_1:FT8KQXNM". Which would suggest it did find the device.
If I start the GUI without the device plugged in, the GUI starts in SIMULATION mode, plugging in the device after doesn't seem to do anything.
I have also tried changing the FTDI driver and using PyFTDI to communicate with the device, but no matter what I do, the device returns FFFF to all queries.
P.S. the Schematics listed on the product page do not match the TI board. (the folder for 3683 contains 3664 files) I had to find the proper schematics somewhere on the e2e forums in a random post.