This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7952: ADS7952 REFP and ANALOG INPUT Rise Time Sequence

Part Number: ADS7952

Please allow me to confirm the startup sequence for the ADS7952.
We are supplying 5V to +VA and 3.3V to +VBD. REFP is supplied with 2.5V.
We have confirmed on the E2E FORUM that there is no sequence for +VA and +VBD.

What we want to confirm is the rise sequence of the voltage applied to REFP and the ANALOG Input.
Are there any constraints on the voltage rise sequence for REFP and the analog input voltage?

The part number of the device we are using is ADS7952 B TI 01K CXZP.

Of course, at the point when xCS transitions from H to L and inputs the configuration information from SDI to the ADS7952, REFP has definitely risen to 2.5V.