Part Number: DAC7716
Hi Team,
I have three questions about the DAC7716.
■ Operating conditions
- AVDD = +15 V, AVSS = −15 V
- DVDD = 5 V, IOVDD = 5 V
- VREF = 5 V
- RST = 5 V (reset deasserted during power-up)
- UNI/BIP-A = UNI/BIP-B = 5 V
- LDAC = 0 V
- VOUT-x = RFB1-x = RFB2-x shorted (voltage output mode)
- Hardware gain = ×4
- No series resistor on VOUT
Below are the questions we would like to confirm:
1) RST high during power-up
Is there any risk of latch-up or device damage if the RST pin is already high (reset released) during power-up?
2) No series resistor on VOUT
If the DAC output is directly connected to the load (no series resistor), is there any risk of overcurrent damage, for example in the case of a short to GND or a heavy load?
3) Gain mismatch
If the hardware gain setting (e.g., ×2) and the command register gain setting (e.g., ×4) are different:
- Could this cause device damage?
- How is the actual output voltage scale determined in this case?
Best Regards,
Shota