Part Number: ADS131M02
Hi,
From the ADS131M02 Datasheet it says that Input Impedance value is 300KoHm.
Can you please specify the Input Impedance Drift (due to Temp.) of this value?
Thanks & Regards
Udi L.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HiUdi L.
The input impedance on this ADC is not a pure resistive input impedance and we do not have a drift specification for 300kohm. The input impedance is related to the modulator frequency and the gain you set, the figure 6-5 in ADS131M02 datasheet shows the plot of input impedance vs. gain in different modes at room temperature. The input impedance for G = 1 to 4 is fairly stable across temperature, but there is a device to device variation. For G >= 8, there is a big swing in the impedance measurements and the input current can go in either direction.
BR,
Dale