This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DDC2256A: Confusing statement about FCLK_MOS register

Part Number: DDC2256A

Thats a screenshot form the DDC2256A datasheet page 32. As the register 0x3A is initialized with 0x00, it seems that the FCLK is normally a CMOS output (as in description 0: FCLK is CMOS signal). Is that correct? In the typical application it is a LVDS singal, which makes sense as DOUT and DCLK are as well. 

So does this bit explicitely has to be set to have FCLK as a LVDS or is it somehow a typo?

Screenshot 2026-02-10 121222.png