Part Number: BP-DAC11001EVM
I am using BP-DAC11001EVM. I encountered serious issues with the J20 header connection. According to the user guide Table 5, it explicitly says that out of 3 pins, PIN-3 is connected with REF_PWR (J18) through L8 inductor, and similarly, it is stated that PIN1 is connected with VCC (J12) through L3 inductor, which can also be verified on Figure 19. However, upon checking the PCB Gerber files, the connection of PIN1 is connected with VDD (J14) through L5 inductor, and physically verified the same using a mutimeter. I am also attaching the images of the gerber files showing the connection of J20 header verifying my claim. 

Circuit_1.1.pdf