Part Number: AFE5809
Other Parts Discussed in Thread: CDCE72010, , LMK04821, LMK04826, CDCM7005, CDCM1802
Hello TI Team,
We are planning to use the AFE5809 for our ultrasound product development prototype.
We would like clarification regarding the ADC clock input configuration:
-
For the ADC clock input, can we directly use an external clock generator or buffer?
-
Is it recommended to use the CDCE72010 to drive the ADC clock?
-
If the CDCE72010 is used to drive both the ADC clock and the CW clock simultaneously, are there any performance concerns or limitations we should be aware of?
-
For the ADC clock, is it acceptable to use a 40 MHz oscillator similar to the one used on the AFE5809EVM, or would you recommend using a dedicated clock buffer/generator such as the CDCE72010?
We would appreciate your guidance on the recommended clocking architecture to ensure optimal performance.
Best regards,
Harsh Shirke