This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS6142: ADC appears to be initiating conversion on the falling clock edge

Part Number: ADS6142

I am using the ADS6142 in an application where I have an event that is synchronized with the ADC input clock so that I expect consistent results in the sampled output data stream. After struggling to build an rough model of the ADC behavior  and interaction with the analog front end for my FPGA test bench, I realized that the sampled data timing was not what I would expect given the relative timing of the signals. I am operating at 12MHz with a 62.5ns event, so it is fairly obvious to correlate the event behavior with the data stream, and the only conclusion I can draw from the data is that the ADC is intiating conversion on the falling edge of the ADC input clock, not the rising edge. I have tested and observed the same behavior when operating at 24MHz, and also managed to get an FPGA model that matches my actual circuit behavior if I assume a falling edge conversion. I have validated the clock polarity as well. The data sheet very clearly states the conversion happens within 2.5ns fo the rising edge. Can you please confirm that this is actually the case?

  • Hi Katie,

    I will see if there is anyone I can reach out to from design. This device is pretty old and I am not sure who might be around to confirm. Please give me a few days to get back with you.

    Just a few questions:

    Are you taking these measurements on your own board design or a TI EVM?

    If your own board design, could you please send me a copy of your schematics?

    Regards,

    Rob

  • This is from my own board, but the measurements I was taking (input clock and differential signal input) are the direct signals going into the ADC as well as the continuous digital data output stream of the ADC. I am running the ADC in CMOS mode at 3.3V on both the digital and analog side and driving the input clock with a single ended AC coupled signal as per the data sheet. I will send you the relevant parts of the schematic.