Part Number: AFE1594
Want to measure bio signal of around 10 - 50uV peak, bandwidth roughly 100Hz. Looking at the AFE1594 but the noise in 150Hz BW chews up most of the dynamic range here so can anything be done with this device? Is there anything similar with better noise? Could oversampling be done? Would the device would work well with a pre-amp (lead-off, resp, PACE function not required)? What sort of amplitude/BW was envisaged for the Audio Evoked Potentials mentioned?