This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8671: Small Package

Part Number: ADS8671
Other Parts Discussed in Thread: ADS7056, ADS7883

Hi,

Is there a product in a smaller package than the ADS8671 that satisfies the following specifications with the conversion timing and no latency similar to the figure below? I am looking for a replacement for the LTC2313ITS8-14 and would like a product in a smaller package with similar specifications.

<specifications>

sampling rate: 1MSP or more, SPI, SAR, Short conversion time

image.png

image.png

Best Regards,

Nishie

  • Hi Nishie, 

    The ADS7056 will be the best cross to the LTC2313-14. It has similar performance and its about 75% smaller then the LTC2313 device. I provided a simple comparison below.

    -Kyle

    Competitor or TI? TI Competitor
    Parameter ADS7056 LTC2313-14
    Description 14-bit 2.5-MSPS ultra-low-power ultra-small-size SAR ADC with SPI 14-Bit, 2.5Msps Serial Sampling ADC in TSOT
    Resolution (Bits) 14 14
    Sample rate (max) (ksps) 2500 2500
    Number of input channels 1 1
    Interface type SPI SPI
    Architecture SAR SAR
    Input type Single-ended Single-Ended
    Multichannel configuration 0 N/A
    Rating Catalog Catalog
    Reference mode Supply External / Internal
    Features Small Size ADC Reference
    Operating temperature range (°C) -40 to 125 -40 ~ 125
    Price|Quantity (USD) 3.3 9.63
    TI functional safety category   N/A
    Package type X2QFN 8-Lead SOT-23
    Pin count 8 0
    Package area (mm^2) 2.3 8.1
    Package size (L x W) (mm) 1.5 x 1.5 N/A
    Power consumption (typ) (mW) 3.5 18.0
    SNR (dB) 74.9 77.5
    Status ACTIVE ACTIVE
  • Hi Kyle-san,

    Thank you for your support.

    Some customers use intermittent operation (samples A and A+1 are not sampled continuously). In this operation, the data output after sampling A+1 should be A+1. I thought the ADS7056 could not do this operation. Is it actually possible?

    The LTC2313-14 can do this operation, and this operation is important in the customer design.

    Also, do you have a product that meets the requirements so far and supports AVDD and DVDD=5V?

    Best Regards,

    Nishie

  • Hi Nishie-san, 

    The ADS8671 or ADS7883(12-bit, 3MSPS, small 6-pin SOT23 package) are the best crosses in this case. 

    -Kyle

  • Hi Kyle-san,

    Am I correct in understanding that there is no product in a smaller package than ADS8671 when 14bit is required?

    Best Regards,

    Nishie

  • Hi Nishe-san, 

    That is correct, the smallest device is the ADS7056, but as previously discussed that device won't work.

    -Kyle