Part Number: ADC12DJ3200
Other Parts Discussed in Thread: LMK04828
Dear Technical Support Team,
I'm considering a solution based on JESD204B Subclass 1, using a combination of Zynq UltraScale+ and a suitable ADC.
I'm are currently focusing on two ADC12DJ3200, which supports JESD204B and can be used in a 4-channel ADC configuration.
Our questions are:
Is it possible to achieve high-accuracy channel-to-channel synchronization using ADC12DJ3200?
I aim to perform ADC with multiple channels (4ch) synchronized using ACD for RF signals in the 1.5GHz band. It is necessary to synchronize the sampling timing of the multiple ADCs with high precision.
Specifically, we want to synchronize the sampling timing of each channel to within 1/4λ to 1/16λ (150ps to 37.5ps) of 1.5GHz.
I aim to minimize the difference in the “sampling instant” of the ADC input as much as possible.
I understand that Subclass1 achieves channel-to-channel synchronization at the tens-of-picosecond level, and that tADJ (time adjust) allows delay tuning with approximately 19 fs resolution.
Therefore, we believe that very fine alignment should be possible in theory, but we would like to confirm whether this is achievable in practice with ADC12DJ3200 in a multi-channel configuration.
Any guidance, limitations, or recommended architecture would be greatly appreciated.
Best Regards,
ttd