Part Number: ADS1299EEGFE-PDK
Other Parts Discussed in Thread: ADS1299
Hi Experts,
I am posting on customer behalf.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS1299EEGFE-PDK
Other Parts Discussed in Thread: ADS1299
Hi Experts,
I am posting on customer behalf.
Hi Marvin,
Please ask the customer to check how the EVM has enumerated in Device Manager. They may need to update the device drivers manually.
We have not updated the EVM SW since its initial release; however, many customers and I are able to use the GUI without issues on Windows 10 and Windows 11.
Regards,
Ryan
Dear Ryan
Thanks a lot for your message.
Please find the details of the debugging process we have performed, Still issue isn't resolved yet.
1. Uninstalled & re-installed all the drivers & kit setup SW - Still observe the GUI to hang & become non-responsive with "e" being displayed on its 7 segment display. However the win10 device manager could correctly enumerate it as NI VISA MMB0 device
2. Connecting only the carrier board with the PC (ADS1299 stack up board removed) the same GUI behaviour is observed
3. If only the GUI runs then there is no hang, which implies that there is issue in the interaction between the kit with the PC.
Hi As a follow-up would like to provide these additional screenshot as well We tried without the HW, then the GUI shows 2 pop ups (screenshots attached) of Firmware load issue warning & shuts down shortly thereafter

The Conditions of the GUI regiser map is never updated even if we input the values
We are also observing that U21 Part is getting warm. Any suggestions. Is this related to GUI interface ?
Hello Dr. Jallapally,
What is powering the MMB0? Have you connected a DC wall adapter that meets the requirements in section 9.4 of the User Guide? Typical wall supply specs are 6V and at least 500mA output.
Without connecting EVM daughterboard to the MMB0, can you test the following?
Then, disconnect power, and plug the two boards back together with the EVM in the default jumper configuration according to section 2.5. Then, re-apply power to the MMB0 and measure the following:
Lastly, please share a high-res photo of your EVM kit, showing their orientation and jumper settings.
Regards,
Ryan