Part Number: ADS7067
Other Parts Discussed in Thread: OPA325
Hi,
we use the ADS7067 in one of our applications. For the most connected analog signals we use the OPA325 as input buffer, but for some slow changing (nearly constant) signals we simply use a RC filter at the analog input. The values of the RC-filter are 10k and 100nF. In addition, there is the kickback RC filter directly at the input of the ADS.
Measurements show that there is a voltage drop over the 10k of appx. 50mV which indicates that there is a leakage current of appx. 5uA.
Is it possible that there is a input leakage current at the analoge inputs of the ADS because I do not find something about it in the datasheet.
Before the ADS is configured by the CPU there is no leakage. Maybe there is some dynamic leakage phenomena.
Design details:
-Reference voltage of ADS7067: 5V (external REF195)
-Supply voltage: AVDD 5.2V; DVDD 1.8V
-Sample rate: 500kSamples/s
-number of used channels: 8
-mode: auto-sequence mode
-Kickback at all inputs: 180R/680pf