Part Number: AMC7908
I'm asking a query for AMC7904RGER, as this particular P/N was not available in dropdown list. I'm doing MTBF and I'm not able to find the maximum current Ic through the transistor that is connected to D+ and D- pins of the IC. Pls provide Vbe or Ib or the maximum collector current that will flow through transistor during sensing of temperature so that I can find the CSR.