Part Number: DAC63004
Hi TI,
DAC63004 specs section 7.4.5.1.2 Programmable Slew-Rate Control reads:
"The slew rate control feature allows the user to control the rate at which the output voltage (VOUT) changes. When this feature is enabled (using the SLEW-RATE-X[3:0] bits), the DAC output changes from the current code to the code in the DAC-X-MARGIN-HIGH or DAC-X-MARGIN-LOW registers"
Do I understand correctly that Linear Slew Mode and Logarithmic Slew Mode work only when the output is being enabled or disabled, and the output value changes to either margin-low or margin-high? In other words, is it true that these modes do not apply when I change the nominal output value by modifying the DAC-X-DATA register?
Needless to say, by modifying the DAC-X-DATA register I can achieve any slew rate in firmware. However, I was hoping this could be done automatically by the DAC, without sending many extra bits and keeping the MCU busy.
Thanks,
Thomas