Part Number: ADS1292R
Other Parts Discussed in Thread: ADS1292
We are developint an AED (battery powered). The device includes the TI ADS1292R. Operations are working and our product passes its POR Self-Test consistently. In the AED we perform a WEEKLY Self-Test which in a few devices fails the check for ECG Data Acquisition. In particular, it fails on the ECG Test signal. The failure seems to be intermittent, but occurs on only a few devices. We have managed to capture the 1292 test signal during a failure and are trying to determine a cause for the failure because the collected signal is defective.
I attempted to upload an image of the plot and Excel Spreadsheet with the plot, but both failed. Here is a VERY rough text approximation of the plot:
........----........---
......./....\....../...
....../......\..../....
...../........|.--.....
..../.........|/.......
---/...................
It shows the critical point we are concerned about. We do not think it is a software issue on our side, since we have sent both generated sine wave and simulated ECG rhythms to the AED and collected correct data. But we are puzzled how any possible noise could disrupt the internal ASD1292R test signal.
Thanks for any suggestions. We will continue debugging on our side.
Ed