This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DDC112: Absolute maximum input current to Analog Input on DDC112

Part Number: DDC112

Hello, we have an application for a DDC112 where we need to know the absolute maximum input current to the Analog input, prior to damaging the part.  We have an application where the part may encounter brief high power inputs to a photodetector, which will translate to a maximum of 9.5mA for under 1mS into the DDC112 analog input.  We do not need to accurately read that value, but we do not want the part damaged.  Thanks for your help.