Part Number: ADS8509
Hello,
I have a design with an ADS8509 A/D where due to non-optimal PCB layout the input voltage at R/Cbar input overshoots to 6.5V for about 5ns after a rising edge. HyperLynx signal integrity simulations with the proper ibis models show about 12mA of current flowing into the R/Cbar input during these overshoots for ~5ns.
Do ADS8509 digital inputs tolerate this transient input current for 5ns? If so what is the maximum transient current that can flow into a digital input, through an ESD clamp diode and into a positive or negative power rail for short period of time (like 5ns or so)?
Thanks,
Naiden Spasov