Part Number: AMC0106M25
Dear TI,
we're using the AMC0106M25 isolated ADC in our isolated Wired M-Bus interface project.
On the isolated side, the AMC0106M25 is measuring the current flowing through the M-Bus via a low-side shunt resistor. On the non-isolated side, the DOUT and CLKIN are interfaced with the MCU (RP2040) via 47R series termination resistors.
On our prototype we have been puzzled by the behaviour of the AMC0106M25 with respect to temperature changes. We have noticed an increase in measured current values when the PCB or the chip became warm. Even relatively small temperature increases (e.g. warming the chip with a finger, etc.) started showing exaggerated current measurements.
We managed to work around the problem by soldering a 47pF/0402 ceramic capacitor between the CLKIN pin and DGND. This seemed to help with the temperature drift problem, although we are not able to explain why. Do you have any ideas?