Part Number: ADS1675
Other Parts Discussed in Thread: PSIEVM
I have a working ADS1675 design, and I'd like to quantify performance of the ADC and my amplifier. I'm feeding a test signal from an Agilent Function Generator, but I suspect its output SFDR is less than the ~103dB specified dynamic range of the ADS1675 running at 2MSPS. I'm seeking recommendations for an effective test setup to fully quantify the dynamic range of my hardware. Is there a recommended function generator? Some way to filter the function generator's output? Anything related to test setup would be appreciated. Thank you!