Part Number: DAC11001B
Other Parts Discussed in Thread: UNIFLASH, CCSTUDIO, BP-DAC11001EVM
Hi Team,
I"m working on DAC11001B precision DAC EVAL kit with launch pad board. I tried to load the bin file in CCStudio Uniflash desktop version and loaded the image successfully as in the attached snapshot. When I tried to launch the DAC GUI, it shows that my HW is not connected [as attached in the snapshot] and for common reference I took the EVAL connected to the Launchpad board. Kindly let me know if i need to do any update in SW or HW wise.
Also, I would like to know if I need to supply external voltage from any source meter to the DAC EVAL or in the launch pad boards. If external supply is required let me know what voltage and where its should be connected/supplied [J12/J14/J16]. Also, on which register should I write the value that make DAC to force 1mV to 10mV and where is the output supply channel pins are present in the DAC EVAL board.
This shall help me to make correction in my setup and get the output as expected. Thanks.