This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC32RF55EVM: Enquiry on ADC32RF55EVM RF input and Clock input

Part Number: ADC32RF55EVM
Other Parts Discussed in Thread: ADC32RF55

Ti team,

 

We have procured the ADC evaluation board for the ADC32RF55 (Dual Channel, 14-bit, 2.6–3 GSPS RF Sampling Data Converter).

We have a few clarifications regarding its operation:

  1. Input Power:
    We understand that the full-scale input is specified in terms of differential voltage/power. Could you please confirm the equivalent single-ended input power range (in dBm) for optimal performance?
    External Clock Requirement:(I have asked this in two of the forums but I didn't get a proper response)
  2. Clock Input Specifications:
    If an external clock is required(when an external clock source is used), please provide the suitable input range in terms of:
    • Power level (dBm)
    • Voltage level (Vpp)
    • Supported clock type (e.g., sine wave, LVPECL, CML, etc.)

Your guidance on the above points will help us in properly configuring and operating the evaluation board.

Looking forward to your response.

Regards,
Sudarshan M