Part Number: ADS122S14
I have an unusual application where I need to measure the resistance of heater banks in a system. The heaters will be run live, and then a couple of times a day - be electronically isolated from the supply and a resistance measuring system switched in - to make sure that the heaters are still working correctly and are the same resistance as when they were initially commisioned.
This is a replacement for a system that was originally designed using a DMM chipset made by Cyrustek using ES51932. This legacy device measured resistance and sent the result out via RS232. We need to design a replacement system that does the same - using an ADC and a processor, to a sufficient resolution.
The solution needs to have the dynamic range to cover 30 ohms to 10 killo ohms
We need to handle two extremes. At one end, we must detect a 6W failure in a full 1200W load, which is a shift of only 0.17 ohms to 0.22 ohms somewhere accross the range (depending on voltage, controller can operate between 200-230VAC). At the other end, we may be measuring single 6W heaters where the base resistance is as high as 8.8 killo ohms.
The solution must resolve 0.01R steps without ‘flicker’ accross the entire range.
Do you have any application notes on using ADC's as resistance meters, or can you suggest a means of achieving this (we are not fixed on this ADC - and can consider alternatives).
Many Thanks
James