This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12QJ1600EVM: Question on Using FDA for DC-Coupled Input with ADC12QJ1600EVM

Part Number: ADC12QJ1600EVM
Other Parts Discussed in Thread: LMH5401, THS4541, ADC12QJ1600

Hi,

I am considering using a fully differential amplifier (FDA) to convert a single-ended input into a differential signal so that I can interface directly with the ADC EVM. I am looking at two options: the THS4541 (with its evaluation board) and the LMH5401 high-speed amplifier.

I previously attempted to capture data using a single-ended input after modifying the ADC EVM as suggested in the forum. However, I am observing overrange on that channel (Channel A) and am unable to retrieve data through the FPGA. In contrast, I am able to capture AC-coupled signals correctly on the other channels (i.e., Channel B).

According to the ADC EVM documentation, DC-coupled differential input is supported, provided that a fully differential amplifier is used to set the common-mode voltage to 1.1 V. Given this, I wanted to confirm whether using either of these FDAs would be appropriate for my setup. Both seem to meet the bandwidth requirements of my signal.

Best regards,
Shariful