This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC60508: Max source/sink current

Part Number: DAC60508

Hello,

I need 25mA + margin(min 3mA) sink and cource current when the output is more than 3V.

In the figure 36 of the datasheet, it seems that DAC60508 can provide up to 40mA source and 30mA sink current. However, I cannot find the specification in the table of the section 7.5.

What is the max sink/source current in number?

Best Regards,