Part Number: ADS8681WEVM-PDK
Other Parts Discussed in Thread: ADS8681
Dear Technical Support Team,
I have a question regarding the schematic for the ADS8681 series evaluation board (ADS8681WEVM-PDK Evaluation Module).
This is related following my post.
Q1
It appears that AVDD is regulated by the TPS7A4901DGNR and is set to 5.01V, but the circuit for DVDD seems to operate on the USB voltage (5.5V?).
Since this is below the absolute maximum rating of 7V, I don’t think it will cause a failure, but DVDD > AVDD, which is outside the recommended range. Is this acceptable?
Q2
since AVDD is generated from the USB power supply for DVDD, I believe DVDD will always be higher than AVDD at power-up due to startup delay.
Since this also does not exceed the absolute maximum rating, can I assume this is acceptable?

Best Regards,
ttd