This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How tester works

Testers which are used for testing voltage at some plug (more like a screw driver with leon lamp & external metal tail), when you insert it in a plug & touch external metal point LED glows giving indication about voltage present. If you don't touch metal it won't glow even if it is in plug having voltage.

  • I want to know how lamp glow when I touch the metal.How does the circuit gets completed. Even if sit on plastic or wooden chair, it still works same way?
  •  Some people say, current gets on your body for 8ms (0.5/60 Hz) & next 8ms it gets off. Then how does it works in dc.
  • Some say body is capacitor which stores charge. Then even if there is no return path for current, i.e I am standing on wooden chair. then how would it store charge. Further comment is capacitor is like  a break in wire. It store charge anyways. But I tested by connected +ve leg of capacitor to +ve of dc supply only & left open -ve leg of cap. It don't get charged. That means cap neads return path to be charged.

I tested current when put in 220V ac by connecting FLUKE ammeter between & current  comes 17 to 18 uA ac.

But then I connected it to 100Vdc. Although light was dim, my ammeter showed 0 uA dc. might be due to precision problem in meter.