This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC128S102-SEP: Radiation Test Reports (TID and SEE)

Part Number: ADC128S102-SEP

Hi Team,

Posting on behalf of our customer.

I'll share this E2E post with our customer so he can reply when needed.

The datasheet for the ADC128S102-SEP states: 

7.3.4.1 Total Ionizing Dose Testing and qualification of these products is done on a wafer level according to MIL-STD-883G, Test Method 1019.7. Testing is done according to condition A and the extended room temperature anneal test described in section 3.11 for application environment dose rates less than 51.61 rad(Si)/s. Wafer level TID data are available with lot shipments.

7.3.4.2 Single Event Latch-Up

One-time single event latch-up (SEL) was preformed according to EIA/JEDEC Standard, EIA/JEDEC57. The linear energy transfer threshold (LETth) shown in the Features section is the maximum LET tested. A test report is available upon request. 

Please share example of wafer level TID data for an example lot as well as the SEL test report.

Regards,

Danilo