I am looking at using the VCA 2615 to amplify a signal with a carrier frequency between 200 kHz and 1 MHz. This signal would be sampled by a 16 bit A/D converter after the VCA 2615. In the data sheet it says that it is recommended for 10 and 12 bit systems. Looking at the data sheet, it should have low enough noise levels and low distortion for a 16 bit system. Is there any reason that the VCA2615 would limit the performance of a 16 bit A/D converter?
Thanks,
Pavel