This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8684: ADS8684 External Reference (/REFSEL, REFIO) behavior during power-up

Part Number: ADS8684

Hi team,

I am evaluating the ADS8684 (ADS868x family) and have questions regarding the external reference configuration and its behavior during power-up.
Background:
  • External reference is applied to the REFIO pin.
  • /REFSEL is tied to DVDD as shown in datasheet section 8.3.8.2 “External Reference” and Figure 62.
  • Internal reference is disabled by /REFSEL = High.
Questions:
  1. During power-up, when /REFSEL is tied directly to DVDD, is there any condition where the internal reference could be briefly enabled before /REFSEL is recognized as High?
    In other words, is there any possibility that the internal reference output and the external reference applied to REFIO could conflict momentarily during DVDD ramp-up?
  2. If REFIO is driven by an external reference while AVDD = 0 V (for example, AVDD ramps after the reference is already present), is this condition supported?
    • If supported, are there any constraints such as maximum injection current, required series resistance, or ramp-rate considerations?
    • If not recommended, what is the preferred power-up sequencing between AVDD, DVDD, /REFSEL, and external VREF?
  3. If the /REFSEL pin is left floating (not connected), is its logic state defined internally?
    • Does it default to internal reference or external reference mode, or is this considered an undefined condition?

Best Regards,
Ryu.