Part Number: ADS131E08
Per Data Sheet (SBAS561C) Fig 37, the third byte of the status word contains GPIO[7:4] (presumably referring to the GPIO register (20)). This uses 4 bits to define an 8-bit byte, so I want to make sure what it means.
Observed behavior is that GPIO[7:4] appears as bits [3:0] (low nybble) in that status word byte. The high-order nybble seems to always read as 0xF0 (but maybe I'm not watching closely enough).
My notion is to put a "well known" bit pattern into the GPIO register and use the status word to detect whether the ADC has been Reset. I'll be using a fairly heavy hammer if that happens (presumed rare), so I want to get it right.
Is it correct that GPIO[7:4] appears as bits [3:0] in the third status word byte? Is there any useful information in bits [7:4] of the third status word byte?