Part Number: ADC12DJ5200RF
Hi team,
My custoemr would like to use the ADC12DJ5200RF under the following conditinos, but he is having trouble linking it to the FPGA(KintexUltrascale+ XCKU11P, JESD IP: JESD204PHY+JESD204C).
- Not using the SYNC pin
- No FEC(CRC12)
- JMODE=0x1F
[Questions]
- To establish connection between the FPGA and the ADC, is following initialization setup explained in the datasheet p191 sufficient?
The custoemr understandas that for JESD204B, in addition to initializing the ADC, a separate "link-up start" step is required. For JESD204C, is the link-up peformed automatically? - He checked communication between JESD204PHY → JESD204C using ILA as shown in below.
Does this indicate the initization has failed?
The JESD204 PHY is asserting rxblock_sync, and the rxheader is showing either 1 or 2, which is normal, and the data rxdata[63:0] is also toggling.
The JESD204C is not asserting the data‑enable signal (c12_axis_tvalid in below) .
Best regards,
Shota Mago