This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLA2024: Datasheet I2C address issue

Part Number: TLA2024

On page 13 of the datasheet, section 13, Table 2, the SLAVE ADDRESS notation is prone to potential errors of taking notice of the hex address representation. The reason: the gap in the binary notation on the false place. If the gap would be inserted left of the lower four bits, one would immediately notify the corresponding hex address: 0x48, 0x49 and third: 0x4b (instead of false 0x90, 0x91 and 0x93).

I'd guess that the author of this datasheet section itself may be confused by the fact that the byte in which the I2C-address is transferred contains READ/WRITE bit as LSB, and hence the upper 7 bits as address.

I'd suggest to modify this small bit of change simply for convenience.

Datasheet revision online is: initial (2017).