Part Number: AFE7950EVM
Other Parts Discussed in Thread: TSW14J58EVM
Hello,
I am using the AFE7950EVM together with the TSW14J58EVM, using Latte only for board configuration (without HSDC Pro).
My goal is to perform measurements involving both TX and RX paths, and more specifically to acquire data simultaneously from two RX channels in a synchronized manner.
I currently use the Latte GUI acquisition function to start the capture and export the data to a CSV file. However, regardless of the RX configuration, the generated CSV file always contains data from only one IQ receiver channel.
The main interest of these evaluation boards for my application is the time synchronization between TX and RX channels, allowing offline signal processing and coherent analysis across multiple receivers.
Could you please advise on the correct configuration or acquisition method to simultaneously save multiple RX IQ channels into the same capture (for example RXA and RXB, or more RX channels if supported) when using Latte only?
Is there a specific Latte configuration, capture setting, JESD configuration, or export procedure required to enable multi-channel synchronized RX recording?
Thank you very much for your support.
Best regards,