Part Number: DAC39RF10-SP
Hello,
I have a few questions regarding DAC39RF10-SP.
1. Could you confirm whether the package uses a ceramic or organic substrate?
ACL0256A ACL (S-PBGA-N) 4229409
2. Is this device compliant with MIL-PRF-38535 Organic Class-Y?
3. Regarding screening and QCI:
We found some information in the following document:
DAC39RF10-SP Production Flow and Reliability Report (Rev. A)
Do you have more detailed information, such as:
- Sample sizes (lot size / number of units tested)
- Screening flow
- Test conditions and acceptance criteria
Any additional documentation would be appreciated.
Best regards,
Koji