Part Number: ADS7038
Hi!
I am trying to start ADC in auto-sequence mode with CRC.
Fix pattern is turn on to check the data. CRC_EN bit is set in the GENERAL_CFG.
Then I read 4 bytes and permanently receive A5 A0 30 00. Is it correct? I expected that CRC should be in 4th byte. Like A5 A0 00 <CRC>.
Next, if I append channel ID, I received A5 A5 2B 00. I expect A5 A5 00 <CRC>.
And finaly, I add OSR and receive A5 A5 2B 00 also. But with OSR turn on, the data should bi 16 bits length. The CRC is not on the 4th byte position. I expect smth like 0A 5A 50 <CRC>.
If I am right, CRC should be in the 4 byte? Help me to understand, please.