This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8319: Altenative ADC

Part Number: ADS8319
Other Parts Discussed in Thread: ADS8862, ADS8685W, ADS8685

Dear Technical Support Team,

Do you have latest devices to replace ADS8319(1ch/16bit/500ksps) + REF5045(4.5V) with alternative ADC ?

ADS8862 seems to be good option, but not latest ADC(2013 RTM).

ADS8685W and ADS8685 has 0-5V input, but these are accept only 4.096V and internal LPF is only 15kHz and 500kHz(it seems to place external LPF to remove aliasing )

Best Regards,

ttd