Part Number: TSW14J58EVM
Other Parts Discussed in Thread: AFE8192EVM,
Hello TI Team,
I am using the AFE8192EVM together with the TSW14J58EVM in a Latte-based environment.
I would like to know whether it is possible to output an external synchronization signal that is synchronized with the start of TX waveform playback initiated by sendCustomComplexData.
In particular, I would like to confirm whether the following signals can be output from the SYNCA / SYNCB / SYNCC connectors:
1. A continuous pulse synchronized with the DAC waveform playback start
2. A clock synchronized with the DAC waveform playback start
If this is supported, could you please provide the following information?
- The Latte command or API name
- The output connector or pin to use
- The signal level
- The pulse width
- The timing relationship between the output signal and the TX playback start
Best regards,